AXIS#.VL.LIMITP
Description
AXIS#.VL.LIMITP sets the velocity command positive limit.
If the input to the velocity loop is higher than AXIS#.VL.LIMITP, then the actual velocity command AXIS#.VL.CMD is limited by the value of AXIS#.VL.LIMITP.
-
-
ECCN 3A255 imposes special limitations on operating speed for induction motors. See Frequency / Velocity Limitation for Open Loop Motor Control.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s See Velocity Units for details. |
Range |
Depends on units. See Velocity Range for details. |
Default Value |
15000 RPM Depends on units. See Velocity Units for details. |
Data Type |
Float |
See Also |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.VL.LIMITP |
5011h |
06h |
Unsigned32 |
Velocity |
- |
Read/Write |
No |
AXIS2.VL.LIMITP |
5111h |
06h |
Unsigned32 |
Velocity |
- |
Read/Write |
No |
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
6032 |
1 |
6032 (0x1790) |
AXIS1.VL.LIMITP |
Signed32 |
Read/Write |
Yes |
71568 |
2 |
6032 (0x1790) |
AXIS2.VL.LIMITP |
Signed32 |
Read/Write |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.VL.LIMITP |
6032 |
Float |
Read/Write |
Velocity |